MOVE.ABORT

Description

MOVE.ABORT stops motor motion and allows continued program execution. Deceleration is determined by CS.DEC.


  • MOVE parameters are only valid when DRV.OPMODE = 2 and DRV.CMDSOURCE = 5.

Example

This program segment commands the motor at constant velocity until input 1 goes to a logic 0. Then, the motor is commanded to stop.

MOVE.ACC = 5000
‘Set acceleration rate equal to 5,000 rpm/sec CS.DEC = 10000 'Set controlled stop deceleration rate to 10,000 rpm/sec
MOVE.RUNSPEED = 120
‘Set Run speed equal to 120 rpm
MOVE.GOVEL
When DIN2.STATE = 0, MOVE.ABORT 'Motor decelerates to a stop at CS.DEC (10,000 rpm/sec)
Print “Move Aborted!”

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1144

No Command No

M_01-05-11-000

Related Topics

Stop | CS.DEC